Feedback_Encoder_Filter_Time

Feedback_Encoder_Filter_Time

Address: 10434 (282CH)
Type: UINT16
Access: Read/Write
Unit:

µs

Range: 0 or 50 to 20000
Default Value: 900 (0.9 ms)
Store Supported: Yes
Description:

This value is used for Feedback feature and define the filter on encoder speed detection.

Value Description

0

Automatic filter activation

50 to 20000

Valid filter value from 50 µs to 20000 µs

In general value from 500 to 2000 are a good choice. If it’s necessary a quicker velocity reaction decrease the value, if it is necessary to reduce the motor noise at very low speed increase the value.

Notes: See Closed Loop Modality for details.